1.6 FLEXCOM ISO7816 SmartCard

This example application shows how to use the FLEXCOM module in ISO7816 mode.

Description

This application configures the FLEXCOM peripheral in ISO7816 mode and performs operation on a SmartCard AT88SC0808C.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/flexcom/usart/flexcom_iso7816_smartcard/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
sam_a5d29_curiosity.XMPLAB X project for SAMA5D29 Curiosity Development Board Kit

Setting Up AT91Bootstrap Loader

To load the application binary onto the target device, the user needs to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
sam_a5d29_curiosity.XSAMA5D29 Curiosity Development Board Kit

Setting Up SAMA5D29 Curiosity Development Board

ADDITIONAL HARDWARE REQUIRED
SETTING UP THE BOARD
  • Connect a programming cable from JTAG connector J12 on board to programmer(J-32 Debugger)
  • Connect programmer(J-32 Debugger) to computer using a micro USB cable
  • Connect the USB port J1 on board to the computer using a micro USB cable (to power the board)
    PinSmartCard Xplained PROMIKRO A5D29 CuriositySAMA5D29 Curiosity Manual Wiring on J25 Connector
    2 (black)GNDGND--
    5 (yellow)CARD_DETECTCSPC4-
    9 (blue)RESETANPD25-
    10 (grey)VCC_ENABLEMISOPC3-
    13 (brown)XCKSCKNo Flexcom on mikroBUS

    PD14 IO02

    J25: 23 FLEXCOM4_IO2

    14 (purple)I/OMOSINo Flexcom on mikroBUS

    PD12 IO0

    J25: 19 FLEXCOM4_IO0

    20 (red)VCC_TARGET+3.3V--

Running the Application

  1. Open the Terminal application (e.g., Tera term) on the computer.
  2. Connect to the USB Serial COM port and configure the serial settings as follows:
    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  3. Build and Program the application using its IDE.
  4. The console displays the following message.