6.2.3.4 rlmdown

Shuts down the license server

Usage:

rlmutil rlmdown [-q] [isv] [-c license_file]

rlmdown shuts down the first license server in the license path RLM_LICENSE. If the -q option is specified, the shutdown happens without a confirmation prompt. If the optional isv is specified, only that ISV's server is shut down.

In order to shut down the RLM server itself, specify the ISV name as RLM. (Note: RLM must be in capital letters).

Note: for Unix systems:

The servers can also be shut down by sending a SIGTERM signal to the RLM process. SIGTERM shuts down all the servers, including RLM.