6.2.3.2 rlmanon

Change user and host names in report log file

Usage:

rlmanon [logfile]

rlmanon reads the report log file logfile, and changes all the user and host names to the form uNNN and hNNN, where NNN is a sequence number. The result is written into the file logfile.anon.

There is a one-to-one mapping from a particular user or host name to its corresponding sequence number, so that reports generated from the log file will accurately reflect the number of unique users and hosts as well as the sharing of licenses. However, actual user and host information is removed from the output logfile.anon.

rlmanon creates a new authenticated report log file if the input log file is an unmodified authenticated log file. If the input file has incorrect authentication records, an error message is generated and no output file is written.

Note: The rlmanon cannot be run via rlmutil.