| 00001000 |
Clears
DMTPRECLR.STEP1, DMTCLR.STEP2 and the Dead Man Timer if and only if preceded
by the correct loading of Pre-Clear Enable (STEP1) in the correct sequence.
The write to the DMTCLR.STEP2 field may be verified by reading DMTCNT and
observing the counter being Reset. |
| all other write
patterns |
The
DMTSTAT.BAD2 flag is set to ‘1’, the value in the
DMTPRECLR.STEP1 remains unchanged and the new value being written to
DMTCLR.STEP2 is captured.Note: These bits 7:0 are also
cleared when a DMT Reset event occurs. |