40.5.2.4 DAC Output on Pin
In the DACCON (DACCON.OUTEN) register, the user can connect the analog output of the DAC to a pin by writing a ‘1’ to the Output Buffer Enable (OUTEN) bit. The pin used by the DAC must have the input disabled from the Port peripheral. There is an output buffer between the DAC output and the pin, which ensures the analog value does not depend on the load of the pin. The output buffer can only source current; it has very limited sinking capability.