12.1.2 NVM Unlock Sequence
The unlock sequence is a mechanism that protects the NVM from unintended self-write programming, sector reads, and erasing. The sequence must be executed and completed without interruption to successfully complete any of the following operations:
- PFM sector erase
- PFM sector write from holding registers
- PFM sector read into write block holding registers
- PFM word write directly to NVM
- DFM byte write directly to NVM
- Write to Configuration Words
| Operation | First Unlock Byte | Second Unlock Byte |
NVMCON1 |
|---|---|---|---|
| Word/Byte write | 55h | AAh | WR |
| Sector write | DDh | 22h | SECWR |
| Sector erase | CCh | 33h | SECER |
| Sector read | BBh | 44h | SECRD |
The general unlock sequence consists of the following steps and must be completed in order:
- Write first unlock byte to NVMCON2
- Write second unlock byte to NMVCON2
- Set the operation control bit of NVMCON1
For PFM and Configuration Word operations, once the control bit is set the processor will stall internal operations until the operation is complete and then resume with the next instruction. DFM operations do not stall the CPU.
Since the unlock sequence must not be interrupted, global interrupts should be disabled prior to the unlock sequence and re-enabled after the unlock sequence is completed.
NVM Unlock Sequence for PFM word write
BCF INTCON,GIE ; Recommended so sequence is not interrupted
MOVF UpperAddr,W ; set the target address
MOVWF NVMADRU
MOVF HighAddr,W
MOVWF NVMADRH
MOVF LowAddr,W
MOVWF NVMADRL
MOVF HighByte,W ; high byte of word to be written
MOVWF NVMDATH ; store in high byte transfer register
MOVF LowByte,W ; low byte of word to be written
MOVWF NVMDATL ; store in low byte transfer register
BSF NVMCON0,NVMEN ; Enable NVM operation
MOVLW 55h ; Load first unlock byte
; –------------------ Required Sequence –-----------------------------
MOVWF NVMCON2 ; Step 1: Load first byte into NVMCON2
MOVLW AAh ; Step 2: Load W with second unlock byte
MOVWF NVMCON2 ; Step 3: Load second byte into NVMCON2
BSF NVMCON1,WR ; Step 4: Set WR bit to begin write
; –-------------------------------------------------------------------
BSF INTCON,GIE ; Re-enable interrupts
- Sequence begins when NVMCON2 is written; steps 1-4 must occur in the cycle-accurate order shown. If the timing of the steps 1 to 4 is corrupted by an interrupt or a debugger halt, the action will not take place.
- Opcodes shown are illustrative; any instruction that has the indicated effect may be used.