12.4.6.3.2 Setup for Using PLL with 8 MHz Internal FRC
The following process is used to set up the PLL to operate the device at 100 MHz with an 8 MHz Internal FRC and configured PLL VCO output to 250 MHz.
- To execute instructions at 100 MHz, a PLL output frequency of 100 MHz will be required.
- To set up the PLL and meet the
requirements of the PLL, follow these steps:
- Select the PLL prescaler to meet
the PFD input frequency requirement.
- Select a PLL prescaler value of N1 = 1.
- FPLLI = 8 MHz
- FPFD = 8 MHz(1/N1) = 8 MHz(1) = 8 MHz
- Select the feedback divider to
meet the VCO output frequency requirement as well as achieve the desired
FVCO frequency.
- Select a feedback divider value of M = 125.
- FVCO = FPLLI x (M/N1) = 8 MHz x (125/1) = 1 GHz
- Select values for the first and
second PLL postscalers to achieve the required FPLLO frequency.
- Select values for the first and second postscalers of N2 = 5 and N3 = 2.
- FPLLO = FVCO/(N2 x N3) = 1 GHz/10 = 100 MHz
- Select the PLL prescaler to meet
the PFD input frequency requirement.
- Writing PLLxCON (can be done in one
PLLxCON write):
- Enable the PLL Input and Feedback Divider update by setting PLLSWEN bit in the PLLxCON register. Enable the PLL Output Divider update by setting FOUTSWEN bit in the PLLxCON register.
- Select a clock source by setting NOSC[3:0] bits in the PLLxCON register to FRC (1).
- Enable clock switching by setting OSWEN bit in the PLLxCON register.
- PLL VCO output setup is optional for a
normal PLL output. PLL VCODIV output is necessary if PLL VCODIV will be chosen as a
CLKGEN input. For a PLL VCO output, the PLLxDIV register needs to be configured. INTDIV
bits of the PLLxDIV register are configured as two.
- FVCO / INTDIV*2 = 1 GHz/ 2*2 =250 MHz
Note: PLL1CON writes written out
for clarity. These writes can be achieved in a single PLL1CON write.
Code Example for Using PLL with 8 MHz Internal FRC
// code example for 100 MHz PLL clock using 10 MHz crystal primary oscillator
//configure backup oscillator in case of failure
//Enable PLL clock generator
PLL1CONbits.ON = 1;
PLL1CONbits.BOSC = 2; //BFRC as backup clock source
PLL1CONbits.FSCMEN = 1; //enable fail safe
//configure PLL values
PLL1DIVbits.PLLPRE = 1; //Reference Clock Divider
PLL1DIVbits.POSTDIV1 = 5; //Post Divider #1
PLL1DIVbits.POSTDIV2 = 2; //Post Divider #2
// PLL Fout = Fin*FBDIV / (PLLPRE * POSTDIV1 * POSTDIV2)
// PLL Fout = 8M*125/(1*5*2) =100MHz
//Enable PLL Input and Feedback Divider update
PLL1CONbits.PLLSWEN = 1;
while (PLL1CONbits.PLLSWEN == 1);
//Enable PLL Output Divider update
PLL1CONbits.FOUTSWEN = 1;
while (PLL1CONbits.FOUTSWEN);
//select clock switching clock source
PLL1CONbits.NOSC = 1; //select FRC clock source
//[1] = FRC - Internal 8 MHz RC oscillator
//[2] = BFRC - Internal Backup 8 MHz RC oscillator
//[3] = POSC - Primary crystal oscillator (4-32 MHz)
//[9] = REFI1 - user definable clock source
//[10] = REFI2 - user definable clock source
PLL1CONbits.OSWEN = 1; //enable clock switching
while (PLL1CONbits.OSWEN); //wait for switching(hardware clear)
while(!OSCCTRLbits.PLL1RDY) //wait for clock to be ready
//configure PLL VCO Divider registers for PLL1 VCO Div clock source
VCO1DIVbits.INTDIV = 2; //integer divide factor
// PLL VCO DIV = PLL VCO clock / 2* INTDIV
//Enable PLL VCO Divider update
PLL1CONbits.DIVSWEN = 1;
while (PLL1CONbits.DIVSWEN);