14.17.9 User ID Memory Window

Some devices have memory locations where you can store checksum or other code identification (ID) numbers. These locations are readable and writable during program/verify. Depending on the device, they also may be accessible during normal execution through the TBLRD and TBLWT instructions.

Figure 14-65. User ID Memory Window with Content

User ID Memory Window Display

Consult your device programming specification to determine what values may be entered here. For most devices, this sets the low nibble of the device ID word; the high nibble is set to ‘0’. The high nibble can be only be written to programmatically, such as by using Table Writes.

In the Standard or Legacy display, data is shown in the following columns.

  • Address – User ID hexadecimal address(es).
  • User ID – Contents (in hex) of User ID memory.

User ID Memory Window Icon

Icons are located on the left side of the window.

Table 14-79. User ID Memory Window Icons
IconIcon TextFunction
FindSpecify a string to find in the window. Select to match whole word or case.
Find NextFind next instance of string from Find.
Find PreviousFind previous instance of string from Find.

User ID Memory Window Menu

Right click in the memory window data area to pop up the menu, as in the table below.

Table 14-80. User ID Memory Window Context Menu
ItemDescription*
Output To FileWrite the displayed window contents to a text file using the Output to File dialog.