14.17.5 CPU Registers Window

The CPU Registers window displays the contents of the SFRs that relate to the device CPU. To view only a few CPU SFRs, you may prefer to use a Watches window, which may help with speed issues when using hardware debug tools (i.e., faster window update rate).

Whenever a break occurs, the contents of the CPU Registers are updated.

Visible Registers

If a data memory register is not physically implemented on a device, it may not appear in the SFR list. Some tools, such as simulators, may allow you to see registers that do not exist on the actual device, such as prescalers.

Single Stepping

If Freeze Peripherals On Halt is selected, the I/O port bits in the SFR or the Watches windows will not update when single stepping. The pin will be modified, but the read request to retrieve the new value is blocked by the freeze and cannot be updated until the next step or run command.

Figure 14-61. CPU Registers Window with Content

CPU Registers Window Display

You may specify how memory is displayed in the window by selecting from the Format drop-down box on the bottom of the window. Choices are:

  • Blank - Only one view.
  • Devices with FPU - For PIC32 devices with a Floating-Point Unit (FPU), the Format options are:
    • All Registers
    • Only CPU Registers
    • Only FPU Registers.

Blank, All Registers or Only CPU Registers Format

Data is displayed in the following columns.

  • Address – SFR physical hexadecimal address.
  • Name – Symbolic name for the SFR.
  • Radix Information – Hex, Decimal, Binary, Char.
  • Virtual – SFR virtual hexadecimal address as defined by the Bus Matrix.

Only FPU Registers Format

Data is displayed in the following columns.

  • Address – SFR physical hexadecimal address.
  • Name – Symbolic name for the SFR.
  • Radix Information – Hex
  • Floating Point – Float, Double

CPU Registers Window Icons

Icons are located on the left side of the window.

Table 14-69. Data Memory Window Icons
IconIcon TextFunction
FindSpecify a string to find in the window. Select to match whole word or case.
Find NextFind next instance of string from Find.
Find PreviousFind previous instance of string from Find.
Go ToGo to specified line number or address.

CPU Registers Window Menu

Right click in the memory window data area to pop up the menu as in the table below.

Table 14-70. CPU Registers Window Context Menu
ItemDescription
Go ToGo to the address/function specified using the Go To dialog.
FindFind text specified using the Find dialog.
Show Register TooltipShow or hide tooltips for a register. Hover over the register name for pop-up information.
Output To FileWrite the displayed window contents to a text file using the Output to File dialog.
PrintPrint the contents of this window using the Print dialog.
Note: If you have a large memory device, the number of pages printed can become very large. A suggestion is to print the window contents to a file (Print dialog, General tab, Print to File check box) and then select which pages from the file you need to print.
Adjust Table ColumnsAdjust the columns automatically.