7.1 Running the Demo on Same Board
(Ask a Question)To run demo on same board, perform the following steps:
- After programming the bit files,
launch the GUI, see the following figure.
Figure 7-3. Displayed GUI - On the Connection tab, point
to COM Port, click Refresh Ports and then click the appropriate (3rd port
corresponding to Flashpro - COM9) COM Port connected to the PC.
Figure 7-4. Com Port Connection - On the Connection tab, click
Connect.
Figure 7-5. Connection Establishment - Check for the connection status at
right bottom corner of the GUI.
Figure 7-6. Connection Status - After successful connection, setup is
ready for the wireless transfer of data. In the Tx Data box, type text data
and click
.Figure 7-7. Data Sent from Transmitter Side - After successful transfer, the
received data must appear in the Rx Data box.
Figure 7-8. Data Received at Receiver Side