3.4.1 Create the Security World
Security World is created with the New-World utility documented in the
nShield Edge and Solo User Guide for Windows. The module must be moved to the
pre-initialization mode.
The new-world utility has the following options:
- -i: Creates a new Security World.
- -m: Specifies ID of the physical HSM module to be added to the Security World.
- -i: Creates a new Security World.
- -Q: Specifies the minimum number of smart cards needed from the ACS to authorize a feature and the total number of smart cards to be used in the ACS. This example has a total of two cards, with only one card needed to authorize a feature.
- -c: Specifies the type of key to use for the new Security World. This example uses the AES key.
The example shown in Figure 3-5 creates a new Security World.
During creation of the Security World, the user is prompted to insert and initialize all ACS cards specified by the -Q option.
Note:
- The values of the
hknsoparameters can be used to uniquely identify the Security World. - If the module is not in the pre-initialization state, creation of the Security
World may encounter an error:
Figure 3-6. Error Message if Module is not in Pre-Initialization State
The new Security World is a file that is created in the following location:
%NFAST_KMDATA%\local
Note: This location also contains all other related security keys.
Once the Security World is created, the module must be moved to the operational mode.