3.4.12 Import the M-HSM Public Keys
The M-HSM server needs to import its own public verify key, so that it can securely remove the
tickets. Use the M‑HSMGenImp utility for import:
M-HSMGenImp -p g4cmsee -i -n g4cm-seespk-<M_UUID> -a pkg-g4cm-seespk-<M_UUID><HEXVALUE> -k g4see- isk
M_UUID: 40 hex characters long UUID for the imported M-HSM public key.
For example, 0000000000000000000000000000000000000002
pkg-g4cm-seespk-<M_UUID><HEX VALUE>: This is the container
file on the disk with the signature verification key to be imported.
For example, pkg-g4cm-seespk-
0000000000000000000000000000000000000002-705f18e9
The resulting file is created in the Security World folder. Information about this key can be viewed using the nfkminfo -k command.
Example of the resulting key file:
key_simple_g4cm-seespk-000000000000000000000000000000000000002
Figure 3-20 shows a sample output from key import.