22.4.2.7.1 Event Capture Action on Events or I/Os
The compare/capture channels can be used as input capture channels to capture events from the Event System or I/O pins and assign them a timestamp. This mode is selected when EVTCTRL.EVACT is configured either as OFF, RETRIGGER, COUNT or START. The following figure shows four capture events for one capture channel.
The TC can detect capture overflow on the input capture channels: If a new capture event occurs while the Capture Interrupt flag (INTFLAG.MCn) is still set, the new timestamp will not be stored, and INTFLAG.ERR will be set.