1.3.3 Verification of Calibration Procedure
Before proceeding to the programmer verification of calibration test, the programmer must pass diagnostic test without any adapter module.
To verify the calibration, perform the following steps:
- Place SM48D or SM48DB on the SS4 programmer, see the following figure.
Figure 1-5. SM48D or SM48DB on the SS4 Programmer
Note: Ensure to note the location of pins 1 (Test pin) and 48 (GND) of the SM48D/SM48DB adapter module (see the following figure) as these pins perform the actual voltage and waveform measurements.Figure 1-6. Test Pin and GND Pin 
- Click Device icon and type BP in the Look for: field.
- Select BP Microsystems SS4 Certificate of Conformance Test option and click Select.
Figure 1-7. BP Microsystems SS4 Certificate of Conformance Test Option 
- Once selected, the following window appears which explains about how to run the test. To close this window, press the Enter key.
Figure 1-8. Test Run Instructions Window 
- Connect the voltmeter probes to pins 1 and 48.Note: Ensure special attention to avoid shorting pin 1 and pin 48.
- To start the test, on the software, click Execute icon.