1.3.3.1 High Voltage Test
To perform high voltage test, follow these steps:
- Measure the voltage of pin 1, see the following
figure. Voltage reading must be within the specified range. Otherwise, the programmer is
out of calibration and needs servicing.
Figure 1-9. Measuring the Voltage of Pin 1
The following figure shows the allowable range of the high voltage test.Figure 1-10. Test Output—High Voltage Test
- To proceed to the next test, on the SS4 programmer, press the START push button.