The INDFn registers
are not physical registers. Any instruction that accesses an INDFn register actually
accesses the register at the address specified by the File Select Registers (FSR). If the
FSRn address specifies one of the two INDFn registers, the read will return
‘0’ and the write will not occur (though Status bits may be
affected). The FSRn register value is created by the pair FSRnH and FSRnL.
The FSR registers form a 16-bit address that allows an addressing space with 65536
locations. These locations are divided into three memory regions:
Traditional/Banked Data
Memory
Linear Data Memory
Program Flash Memory
Figure 9-18. Indirect Addressing
DS40002682A
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.