3.2.6 Reset State Priorities
The Reset State Manager manages the following priorities between the different reset sources, given in descending order:
General Reset
Backup Reset
Watchdog Reset
Software Reset
User Reset
Particular cases are listed below:
- When in User Reset:
A watchdog event is impossible because the Watchdog Timer is being reset
A Software Reset is impossible because the processor reset is being activated
- When in Software Reset:
A watchdog event has priority over the current state
The NRST has no effect
- When in Watchdog Reset:
The processor reset is active and so a Software Reset cannot be programmed
A User Reset cannot be entered