The network tool commands are used for tools not physically connected to the local
computer but through a network via ethernet, wifi, USB, etc. The default is USB.
To display information about the network tool commands for a selected tool available in
the MDB, type help networktool. The table below provides additional
information for this class of commands.
Table 3-5. Network Tool Commands| Command | Description |
|---|
| AddIP | Adds a user-specified newtork tool with the user-specified IP
address. Command format: addip
userSpecifiedIPAddress xxx.xxx.xxx.xxx
Note: The IP address needs
to be in the form
xxx.xxx.xxx.xxx. Example: Addip
192.170.001.001
|
| Confignetworktool | Reads or writes the network settings for the selected
tool. Command format: confignetworktool
[toolType] [index] [read\write]
- toolType - If
MDB is not currently connected to a tool (via the
hwtool command), tooltype must be
supplied (e.g. ice4). Otherwise, toolType should not be
used. - index - The
index of the specific tool (as shown by the
hwtool command). The default index is
zero and will be applied if no index is provided. If MDB is
already connected to a tool (via the hwtool
command), the index parameter should not be used. - read/write -
The read/write parameter is optionial and indicates whether
MDB will read the current network settings off of the tool
or write settings to the tool. Use,
read to
read settings and, write to write settings.
the default is to write the settings and will be applied if
no read/write setting is provided. This setting is valid
regardless of whether or not MDB is currently connected to a
tool (via the hwtool command). However, if
MDB is currenttly connected to a tool (via the
hwtool command), MDB will disconnect
from the tool after a successful write of the network
settings.Use the set command to set each specific
network setting. The syntax for the network settings is
as follows: - Connection Type:
name =
networktool.connection.typevalid
values = ethernet, usb, ethernetstaticip, wifista,
wifiap, (default is usb). - Static IP address:
name =
networktool.static.ipData must be in
the form (x.x.x.x) where x's are
positive numbers from 0 to 255 (default =
0.0.0.0). - Gateway:
name =
networktool.gatewayData must be in the
form (x.x.x.x) where x's are
positive numbers from 0 to 255 (defualt =
0.0.0.0). - Subnet Mask:
name =
networktool.subnet.maskData must be in
the form (x.x.x.x) where x's are
positive numbers from 0 to 255 (default =
255.255.255.255). - Network SSID:
name =
networktool.ssidvalue = any valid
network name (default is an empty
string). - Security Type:
name =
networktool.security.typevalid values
= wep, enterprise, personal, none, (default is
none). - User
Name:
name =
networktool.user.nameAny valid user
name (default is an empty string). - Password:
name =
networktool.password
Any valid password (default is an empty
string).
When writing new settings, MDB performs a read
modify write operation so that only the settings that
have been explicitly declared, through the "set"
command, will be applied to the tool.
|
| RemoveIP | Remove a user-specified network tool with the user-specified IP
address. Command format: removeip
[userSpecifiedIPAddress]
Examples: To
remove a user-specified IP address:removeip
192.170.001.001 To remove all user-specified
network tools: removeip all |