3.2.3.4 How to Add Project Library

Tip:

Ensure you have static library projects in the current solution.

Right click on Project or Libraries Node in the project to invoke the 'Add Library' Wizard.

Select Project Libraries Tab; here, you will see all the static libraries in the current solution listed.

Select the Static Library which you would like to add.

Click OK.

Figure 3-8. View of a Project after Adding Libraries

Also, you will see the added Project → Project Dependencies Static Library.

Figure 3-9. View of a Project Dependencies after Adding Libraries