1.2.11.4.9 SYS_TIME_FrequencyGet Function
C
uint32_t SYS_TIME_FrequencyGet ( void )
Summary
Gets the frequency at which the hardwaer timer counts.
Description
For tick-less mode this API returns the frequency at which the hardware timer runs. For tick-based mode, this API returns the frequency at which the hardware timer generates a periodic tick. This frequency determines the maximum resolution of all services provided by SYS_TIME.
Precondition
The SYS_TIME_Initialize function should have been called before calling this function.
Parameters
None
Returns
If the timer has been initialized and is ready:
- For tick-less mode this API returns the frequency at which the hardware timer runs.
- For tick-based mode, this API returns the frequency at which the hardware timer generates a periodic tick.
Returns 0 if the timer is not initialized.
Example
uint32_t frequency = SYS_TIME_FrequencyGet();
Remarks
This frequency is determined by hardware capabilities and how they are configured and initialized.