1.2.11.4.14 SYS_TIME_CountToMS Function
C
uint32_t SYS_TIME_CountToMS ( uint32_t count )
Summary
Converts a counter value to time interval in milliseconds.
Description
This function converts a counter value to time interval in milliseconds, based on the hardware timer frequency as configured and as reported by SYS_TIME_FrequencyGet.
Precondition
The SYS_TIME_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| count | Counter value to be converted to an equivalent value in milliseconds. |
Returns
Number of milliseconds represented by the given counter value.
Example
Given a previously captured uint32_t counter value called "timestamp" captured using the SYS_TIME_CounterGet function, the following example will calculate number of milliseconds elapsed since timestamp was captured.
uint32_t count = SYS_TIME_CounterGet() - timestamp; uint32_t ms = SYS_TIME_CountToMS(count);
Remarks
None.