1.2.11.4.13 SYS_TIME_CountToUS Function
C
uint32_t SYS_TIME_CountToUS ( uint32_t count )
Summary
Converts a counter value to time interval in microseconds.
Description
This function converts a counter value to time interval in microseconds, based on the hardware timer frequency as configured and as reported by SYS_TIME_FrequencyGet.
Precondition
The SYS_TIME_Initialize function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| count | Counter value to be converted to an equivalent value in microseconds. |
Returns
Number of microseconds represented by the given counter value. |
Example
Given a previously captured 32-bit counter value called "timestamp" captured using the SYS_TIME_CounterGet function, the following example will calculate the number of microseconds elapsed since timestamp was captured.
uint32_t count = SYS_TIME_CounterGet() - timestamp; uint32_t us = SYS_TIME_CountToUS(count);
Remarks
None.