DRV_AT24_Initialize Function
C
SYS_MODULE_OBJ DRV_AT24_Initialize(
const SYS_MODULE_INDEX drvIndex,
const SYS_MODULE_INIT * const init
)Summary
Initializes the AT24 EEPROM device
Description
This routine initializes the AT24 EEPROM device driver making it ready for clients to open and use. The initialization data is specified by the init parameter. It is a single instance driver, so this API should be called only once.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the instance to be initialized |
| init | Pointer to the init data structure containing any data necessary to initialize the driver. |
Returns
If successful, returns a valid handle to a driver instance object. Otherwise, returns SYS_MODULE_OBJ_INVALID.
Example
SYS_MODULE_OBJ sysObjDrvAT24;
DRV_AT24_PLIB_INTERFACE drvAT24PlibAPI = {
.writeRead = (DRV_AT24_PLIB_WRITE_READ)TWIHS0_WriteRead,
.write = (DRV_AT24_PLIB_WRITE)TWIHS0_Write,
.read = (DRV_AT24_PLIB_READ)TWIHS0_Read,
.isBusy = (DRV_AT24_PLIB_IS_BUSY)TWIHS0_IsBusy,
.errorGet = (DRV_AT24_PLIB_ERROR_GET)TWIHS0_ErrorGet,
.callbackRegister = (DRV_AT24_PLIB_CALLBACK_REGISTER)TWIHS0_CallbackRegister,
};
DRV_AT24_INIT drvAT24InitData = {
.i2cPlib = &drvAT24PlibAPI,
.slaveAddress = 0x57,
.pageSize = DRV_AT24_EEPROM_PAGE_SIZE,
.flashSize = DRV_AT24_EEPROM_FLASH_SIZE,
.numClients = DRV_AT24_CLIENTS_NUMBER_IDX,
.blockStartAddress = 0x0,
};
sysObjDrvAT24 = DRV_AT24_Initialize(DRV_AT24_INDEX, (SYS_MODULE_INIT *)&drvAT24InitData);
Remarks
This routine must be called before any other DRV_AT24 routine is called. This routine should only be called once during system initialization.