1.1.13.1 MX25L Driver
This driver provides a non-blocking interface to read, write and erase MX25L Flash memory. The driver uses the QSPI peripheral library to interface with the MX25L Flash.
Key Features:
Supports Multiple variants of the MX25L Flash devices
Supports a single instance of the MX25L Flash and a single client to the driver
Supports Sector/Bulk/Chip Erase Operations
Supports writes to random memory address within page boundaries
The library interface is compliant to the block media interface expected by the Memory Driver. This allows running a file system on the AT25DF Flash using the Memory Driver and the File System Service
The library can be used in both Bare-Metal and RTOS environments