1.1.13.1.3 Configuring The Library
The MX25L driver library should be configured through the MHC. The following figures show the MHC configuration window for the MX25L driver and brief description.
MX25L Driver with QSPI peripheral in SQI mode connected

MX25L Driver with connection to Memory Driver

Configuration Options
PLIB Used:
- Specifies the Peripheral library connected
Number Of Clients:
Indicates maximum number of clients
Always set to one as it supports only a single client
MX25L Start Address:
Specifies the flash memory start address to be used for Transfer operations
The start address will be populated in the device geometry table DRV_MX25L_GEOMETRY
MX25L Erase Buffer Size:
This option appears only when the MX25L driver is connected to the Memory driver for block operations
Specifies the size for erase buffer used by Memory driver
The size of the buffer should be equal to erase sector size as the memory driver will call DRV_MX25L_SectorErase