1.1.12.1 AT25DF Driver
This driver provides a non-blocking interface to read, write and erase AT25DF Flash memory. The library uses the SPI peripheral library (PLIB) to interface with the AT25DF
Key Features:
Supports Multiple variants of the AT25DF Flash devices
Supports a single instance of the AT25DF Flash and a single client to the driver
Supports Sector/Bulk/Chip Erase Operations
Supports writes to random memory address within page boundaries
The library interface is compliant to the block media interface expected by the Memory Driver. This allows running a file system on the AT25DF Flash using the Memory Driver and the File System Service
The library can be used in both Bare-Metal and RTOS environments