DRV_AT25DF_GeometryGet Function
C
bool DRV_AT25DF_GeometryGet(const DRV_HANDLE handle, DRV_AT25DF_GEOMETRY *geometry)
Summary
Returns the geometry of the device.
Description
This API gives the following geometrical details of the DRV_AT25DF Flash:
- Number of Read/Write/Erase Blocks and their size in each region of the device
Precondition
DRV_AT25DF_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| geometry | Pointer to Flash device geometry table instance |
Returns
- True - If able to get the geometry details of the Flash
- False - If handle is invalid
Example
DRV_AT25DF_GEOMETRY flashGeometry; uint32_t readBlockSize, writeBlockSize, eraseBlockSize; uint32_t nReadBlocks, nReadRegions, totalFlashSize; // myHandle is the handle returned from DRV_AT25DF_Open API. DRV_AT25DF_GeometryGet(myHandle, &flashGeometry); readBlockSize = flashGeometry.readBlockSize; nReadBlocks = flashGeometry.readNumBlocks; nReadRegions = flashGeometry.readNumRegions; writeBlockSize = flashGeometry.writeBlockSize; eraseBlockSize = flashGeometry.eraseBlockSize; totalFlashSize = readBlockSize * nReadBlocks * nReadRegions;
Remarks
None.