DRV_AT25DF_Read Function
C
bool DRV_AT25DF_Read(const DRV_HANDLE handle, void *rxData, uint32_t rxDataLength, uint32_t address )
Summary
Reads 'n' bytes of data from the specified start address of Flash.
Description
This function schedules a non-blocking read operation for the requested number of data bytes from the given address of the Flash.
The requesting client should call DRV_AT25DF_TransferStatusGet API to know the current status of the request OR the requesting client can register a callback function with the driver to get notified of the status.
Precondition
DRV_AT25DF_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine. |
| rxData | Buffer pointer into which the data read from the DRV_AT25DF Flash memory will be placed. |
| rxDataLength | Total number of bytes to be read. |
| address | Memory start address from where the data should be read. |
Returns
True:
- if the read request is accepted
False:
- if handle is invalid
- if the pointer to the receive buffer is NULL or number of bytes to read is 0
- if the driver is busy handling another transfer request
Example
#define BUFFER_SIZE 1024 #define MEM_ADDRESS 0x00 uint8_t readBuffer[BUFFER_SIZE]; // myHandle is the handle returned from DRV_AT25DF_Open API. // In the below example, the transfer status is polled. However, application can // register a callback and get notified when the transfer is complete. if (DRV_AT25DF_Read(myHandle, readBuffer, BUFFER_SIZE, MEM_ADDRESS) != true) { // Error handling here } else { // Wait for read to be completed while(DRV_AT25DF_TransferStatusGet(myHandle) == DRV_AT25DF_TRANSFER_STATUS_BUSY); }
Remarks
None.