DRV_AT24_Write Function
C
bool DRV_AT24_Write(const DRV_HANDLE handle, void *txData, uint32_t txDataLength, uint32_t address)Summary
Writes 'n' bytes of data starting at the specified address.
Description
This function schedules a non-blocking write operation for writing txDataLength bytes of data starting from given address of EEPROM.
The requesting client should call DRV_AT24_TransferStatusGet API to know the current status of the request OR the requesting client can register a callback function with the driver to get notified of the status.
Preconditions
DRV_AT24_Open must have been called to obtain a valid opened device handle.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| txData | The source buffer containing data to be programmed into AT24 EEPROM |
| txDataLength | Total number of bytes to be written |
| address | Memory start address from where the data should be written |
Returns
True:
- if the write request is accepted
False:
- if handle is invalid
- if the pointer to transmit buffer is NULL or number of bytes to write is 0
- if the driver is busy handling another transfer request
Example
#define BUFFER_SIZE 1024 #define MEM_ADDRESS 0x00 uint8_t CACHE_ALIGN writeBuffer[BUFFER_SIZE]; // myHandle is the handle returned from DRV_AT24_Open API. // In the below example, the transfer status is polled. However, application can // register a callback and get notified when the transfer is complete. if (DRV_AT24_Write(myHandle, writeBuffer, BUFFER_SIZE, MEM_ADDRESS) != true) { // Error handling here } else { // Wait for write to be completed while(DRV_AT24_TransferStatusGet(myHandle) == DRV_AT24_TRANSFER_STATUS_BUSY); }
Remarks
None.