1.2.6.1 SYS_DMA_ChannelCallbackRegister Function

1.2.6.1 C

void SYS_DMA_ChannelCallbackRegister
(
SYS_DMA_CHANNEL channel,
const SYS_DMA_CHANNEL_CALLBACK eventHandler,
const uintptr_t contextHandle
)

1.2.6.1 Summary

This function allows a DMA client to set an event handler.

1.2.6.1 Description

This function allows a client to set an event handler. The client may want to receive transfer related events in cases when it submits a DMA transfer request. The event handler should be set before the client intends to perform operations that could generate events.

This function accepts a contextHandle parameter. This parameter could be set by the client to contain (or point to) any client specific data object that should be associated with this DMA channel.

1.2.6.1 Precondition

DMA Controller should have been initialized.

1.2.6.1 Parameters

ParametersDescription
channelA specific DMA channel from which the events are expected
eventHandlerPointer to the event handler function
contextHandleValue identifying the context of the application/driver/middleware that registered the event handling function

1.2.6.1 Returns

None.

1.2.6.1 Example

MY_APP_OBJ myAppObj;

void APP_DMA_TransferEventHandler(SYS_DMA_TRANSFER_EVENT event, uintptr_t contextHandle)
{
    switch(event)
    {
        case SYS_DMA_TRANSFER_COMPLETE:
        // This means the data was transferred.
        break;

        case SYS_DMA_TRANSFER_ERROR:
        // Error handling here.
        break;

        default:
        break;
    }
}

// User registers an event handler with DMA channel. This is done once.
SYS_DMA_ChannelCallbackRegister(channel, APP_DMA_TransferEventHandler,(uintptr_t)&myAppObj);

1.2.6.1 Remarks

None.