1.6.3.10 DRV_G3ADP_MAC_PacketTx Function
C
TCPIP_MAC_RES DRV_G3ADP_MAC_PacketTx(DRV_HANDLE hMac, TCPIP_MAC_PACKET * ptrPacket);Summary
G3 ADP MAC driver transmit function.
Description
This is the MAC transmit function. Using this function a packet is submitted to the G3 ADP stack for transmission.
Precondition
DRV_G3ADP_MAC_Initialize must have been called to set up the driver. DRV_G3ADP_MAC_Open() should have been called to obtain a valid handle.
Parameters
| Param | Description |
|---|---|
| hMac | Handle identifying the MAC driver client |
| ptrPacket | Pointer to a TCPIP_MAC_PACKET that's completely formatted and ready to be transmitted over the network |
Returns
- TCPIP_MAC_RES_OK if success
- A TCPIP_MAC_RES error value if failed
Example
TCPIP_MAC_RES res;
TCPIP_MAC_PACKET * ptrPacket;
// The content of the packet must be built accordingly to TCPIP_MAC_PACKET
if(pNetIf->hIfMac != 0)
{
res = DRV_G3ADP_MAC_PacketTx(pNetIf->hIfMac, ptrPacket);
}Remarks
- The G3 ADP MAC driver supports internal queuing. A packet is rejected only if it's not properly formatted. Otherwise it will be scheduled for transmission and queued internally if needed.
- Once the packet is scheduled for transmission the G3 ADP MAC driver will set the TCPIP_MAC_PKT_FLAG_QUEUED flag so that the stack is aware that this packet is under processing and cannot be modified.
- Once the packet is transmitted, the TCPIP_MAC_PKT_FLAG_QUEUED will be cleared, the proper packet acknowledgment result (ackRes) will be set and the packet acknowledgment function (ackFunc) will be called.