1.6.3.13 DRV_G3ADP_MAC_StatisticsGet Function
C
TCPIP_MAC_RES DRV_G3ADP_MAC_StatisticsGet(DRV_HANDLE hMac, TCPIP_MAC_RX_STATISTICS* pRxStatistics, TCPIP_MAC_TX_STATISTICS* pTxStatistics);Summary
Gets the current G3 ADP MAC statistics.
Description
This function will get the current value of the statistic counters maintained by the G3 ADP MAC driver.
Precondition
DRV_G3ADP_MAC_Initialize must have been called to set up the driver. DRV_G3ADP_MAC_Open() should have been called to obtain a valid handle.
Parameters
| Param | Description |
|---|---|
| hMac | Handle identifying the MAC driver client |
| pRxStatistics | Pointer to a TCPIP_MAC_RX_STATISTICS that will receive the current RX statistics counters. Can be 0 if not needed. |
| pTxStatistics | Pointer to a TCPIP_MAC_TX_STATISTICS that will receive the current TX statistics counters. Can be 0 if not needed. |
Returns
- TCPIP_MAC_RES_OK if all processing went on OK.
- TCPIP_MAC_RES_OP_ERR error code if function not supported by the driver.
Example
TCPIP_MAC_RX_STATISTICS rxStatistics;
TCPIP_MAC_TX_STATISTICS txStatistics;
TCPIP_MAC_RES res = DRV_G3ADP_MAC_StatisticsGet(pNetIf->hIfMac, &rxStatistics, &txStatistics);Remarks
- The reported values are info only and change dynamically.