1.6.3.3 DRV_G3ADP_MAC_Status Function
C
SYS_STATUS DRV_G3ADP_MAC_Status ( SYS_MODULE_OBJ object );
Summary
Provides the current status of the G3 ADP MAC driver.
Description
This function provides the current status of the G3 ADP MAC driver module.
Precondition
The DRV_G3ADP_MAC_Initialize function must have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | Driver object handle, returned from DRV_G3ADP_MAC_Initialize |
Returns
- SYS_STATUS_READY - Indicates that any previous module operation for the specified module has completed
- SYS_STATUS_BUSY - Indicates that a previous module operation for the specified module has not yet completed
- SYS_STATUS_ERROR - Indicates that the specified module is in an error state
Example
SYS_STATUS macStat = DRV_G3ADP_MAC_Status(pNetIf->macObjHandle);
if(macStat < 0)
{ // failed; kill the interface
TCPIP_STACK_BringNetDown(&tcpip_stack_ctrl_data, pNetIf, TCPIP_STACK_ACTION_IF_DOWN, TCPIP_MAC_POWER_DOWN);
pNetIf->Flags.bMacInitDone = true;
}
else if(macStat == SYS_STATUS_READY)
{ // get the MAC address and MAC processing flags
...
}Remarks
None.