1.12 Generic Timer Periodic Interrupt
This application shows how to use Generic timer counter in interrupt mode.
Description
This application toggles an LED based off the Generic Timer interrupt. Every time the Generic Timer counter expires the LED toggles. You can start, stop and change period of the timer counter using push button switches.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/generic_timer/led_toggle_interrupt/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a7g5_ek.X | MPLABX project for SAMA7G54 Evaluation Kit |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a7g5_ek.X | SAMA7G54 Evaluation Kit |
Setting Up SAMA7G5 Evaluation Kit
- Connect an oscilloscope to clock output pin
- Connect a 5V power supply to the board. This can be either of the following:
- A USB cable connected between “USBA” (J7) connector on the board and USB host port on PC
- A 5V DC adapter connected to “5V DC IN” (J1) connector on board
- Connect the Debug USB port (J24) on the board to the computer using a micro USB cable
Running the Application
- Build and run the application using its IDE
- Press PB_USER1 switch to start/stop timer
- LED toggles at a fixed rate when timer is on and stops toggling when timer is off
- Timer period can be monitored on clock output pin
- Press PB_USER2 switch to change the timer period
- When timer period is changed LED toggle rate is changed
- Exact period can be measured on the clock output pin
- Timer period cycles between 250ms, 500ms, 750ms and 1000ms
| Board | PB_USER1 | PB_USER2 | LED Name | Clock Output Pin |
|---|---|---|---|---|
| SAMA7G54 Evaluation Kit | USER BUTTON | SW4 | RGB_LED (Blue) | PD20 (PWM pin on mikroBUS2 connector) |