51.7 I2S Application Examples

The I2S can support several serial communication modes used in audio or high-speed serial links. Some standard applications are shown in the following figures.
Note: The following examples are not a complete list of serial link applications supported by the I2S.
Figure 51-7. Audio Application Block Diagram
Figure 51-8. Time Slot Application Block Diagram
Figure 51-9. Codec Application Block Diagram
Figure 51-10. PDM Microphones Application Block Diagram