| Name  | Description  | 
| Introduction | Introduces the MPLAB Harmony USB Human Interface Device (HID)
                                    Device Library.  | 
| Using the Library | This topic describes the basic architecture of the HID
                                    Function Driver and provides information and examples on its
                                    use.  | 
| Configuring the Library | Describes how to configure the HID Function Driver.  | 
| Library Interface | This section describes the Application Programming Interface
                                    (API) functions of the USB Device HID library.Refer to each
                                    section for a detailed description.  | 
| Files | This section lists the source and header files used by the
                                    library.  |