| Name  | Description  | 
| Introduction | This section provides information on library design, configuration, usage and
                the library interface for the USB Audio 2.0 Device Library.  | 
| Using the
                  Library | This topic describes the basic architecture of the Audio 2.0 Function Driver
                and provides information and examples on its use.  | 
| How the
                  Library Works |  This section explains the working of  the Audio 2.0 Function Driver
                Library. | 
| Configuring
                  the Library | The application designer must specify the following configuration parameters
                while using the USB Audio 2.0 Device Driver. The configuration macros that implement
                these parameters must be located in the system_config.h file in the
                application project and a compiler include path (to point to the folder that
                contains this file) should be specified.  | 
| Library
                  Interface | This section describes the Application Programming Interface (API) functions of
                the USB Device Audio LibraryRefer to each section for a detailed description.
               | 
| Files | This section lists the source and header files used by the library.  |