| Name | Description |
| Introduction
| Introduces the MPLAB Harmony USB Host Layer Library. |
| Using the
Library | This topic describes the basic architecture of the USB Host Layer and
provides information and examples on its use. |
| Configuring the Library
| Describes how to configure the USB Host Layer. |
| Library
Interface
| This section describes the Application Programming Interface (API) functions
of the USB Host Layer Library.Refer to each section for a detailed description.
|
| Files
| This section lists the source and header files used by the library. |