| Name | Description |
| Introduction | Introduces the MPLAB Harmony USB CDC Host Library. |
| Using the
Library | This topic describes the basic architecture of the USB CDC Host Client Driver
Library and provides information and examples on its use. |
| Configuring the Library | Describes how to configure the USB CDC Host Library. |
| Library
Interface | This section describes the Application Programming Interface (API) functions
of the USB CDC Client Driver Library. Refer to each section for a detailed
description. |
| Files | This section lists the source and header files used by the library. |