3.8 USB Generic Host Client driver Library
Topics
| Name | Description |
| Introduction | Introduces the MPLAB Harmony USB Generic Host Client driver Library. |
| Using the Library | This topic describes the basic architecture of the USB Generic Host Client driver Library and provides information and examples on its use. |
| Configuring the Library | Describes how to configure the USB Host Layer. |
| Library Interface | This section describes the Application Programming Interface (API) functions of the USB Generic Host Client driver Library. Refer to each section for a detailed description. |
| Files | This section lists the source and header files used by the library |