| Name | Description |
| Introduction
| Introduces the MPLAB Harmony USB HID Host Mouse Driver Library. |
| Using the
Library | This topic describes the basic architecture of the USB HID Host Mouse Driver
Library and provides information and examples on its use. |
| Configuring the Library | Describes how to configure the USB HID Host Mouse Driver. |
| Library
Interface | This section describes the Application Programming Interface (API) functions
of the USB HID Host Mouse Driver Library.The USB Mouse driver does not require
explicit API call by the application to obtain Mouse data. The data in the
appropriate format is sent to the application during an application event handler
function call. |
| Files | This section lists the source and header files used by the library. |