The Data Gateway Interface is available on most kits with an Embedded
Debugger. The DGI control panel can communicate with a DGI device. The
figure below shows the DGI control panel module.
Figure 2-1. Data Gateway Interface
Control Panel
Tip: A new DGI Control Panel can
be opened in External Connection in the
Modules section of the Configuration
tab in the Data Visualizer.
All detected DGI devices are listed in the drop-down list with the kit
name and serial number. Using the Connect button will
connect to the selected DGI device and query for available interfaces. The
available interfaces will be listed under Interfaces.
To enable an interface, check the box next to the name. When an interface is
enabled, the sources and sinks can be connected to other endpoints. The Gear
button is used to configure the interface. See the interface-specific
sections for an explanation of the configuration fields.
To start polling data from the interfaces, click the
Start button. The Reset
MCU check box will cause the MCU to be held in Reset
during start.
The Data Visualizer supports two different protocols for
Auto-configuration; the Atmel Data Protocol (ADP) and the Data Stream protocol. When
using ADP, the configuration resides in the target application code and the target
application sends the configuration settings, upon request, from the Data Visualizer.
When using the Data Stream protocol, the configuration resides in files stored on the
host computer and the target application just sends an ID to identify which
configuration files to be loaded by the Data Visualizer. For more information on ADP,
see Atmel Data Protocol. For more information on the Data Stream protocol, see
Data Stream Protocol.
To enable Auto-configuration the Autodetect
protocols option must be enabled.
After pushing Connect the Data Visualizer
will enable all interfaces while it looks for the ADP handshake message or a Data Stream
Configuration packet. If an ADP handshake message is received, the Data Visualizer will
request configuration information from the target application. If a Data Stream
Configuration packet is found, the Data Visualizer searches through the folders in the
Auto-Configuration search path looking for configuration files with names matching the
detected ID.
Important: To
make sure the Data Visualizer detects the Data Stream Configuration packet, it must
be sent by the target at least twice per second.
Important: Asynchronous
serial protocols (e.g., UART protocols used by DGI USART and CDC Virtual COM port
interfaces) use the following baud rates for auto-detection:
Table 2-1. Baud Rates Used on
Asynchronous Interfaces for Auto-Detection of Protocols
Baud Rate
9600
19200
38400
57600
115200
230400
500000
1000000
2000000
Using any baud rates not in the table will not work for auto-detection of
protocols over asynchronous interfaces (DGI UART and Serial port/CDC Virtual COM
port).
Tip: To see the current
search path used by Data Visualizer to look for configuration files, check the
Show Config search path option.
The search path is a semicolon separated list of paths. When Data Visualizer
detects an Auto-Configuration ID, it will search through the paths in the list
looking for configuration files with the correct file names.
If the Data Visualizer cannot find any valid configuration files it
will show a browser dialog window asking for the path to the folder where the correct
configuration files reside.
After selecting a folder, the folder will be APPENDED to the
Auto-Configuration search path.
Tip: To reset the search path and select a
new single folder as the search path, click the link on the Autodetect
protocols option text.
Data Visualizer will then pop up a browser dialog asking for the path to the
folder where the configuration files reside. The original search path will be
CLEARED and the newly selected folder will be set as search path.
Important: All three
configuration files must reside in the same folder.