This chapter gives an example on how to configure the
Oscilloscope module to be used with a target application
implementing a Night mode switch with a light sensor. Although this example only
utilizes the SPI interface as data source, the procedure will be the same for all data
sources. The target code used in this example and a description of the hardware setup
can be found in Oscilloscope Example Code.
Todo: Select correct tool in the
DGI Control Panel.
Todo: Click
Connect to make a connection to the DGI on the selected
tool.
Todo:
Click the
SPI checkbox
Open the
SPI Configuration dialog by
clicking the Gear button next to the
SPI checkbox
Todo:
Open the configuration
panel
Add an
Oscilloscope module to the Data Visualizer
Drag the
source connector from the interface in the
DGI Control Panel into the
sink for the oscilloscope channel to make a
connection
The Oscilloscope module can now
be used to analyze the data acquired from the light sensor when toggling a desk lamp ON
and OFF above the I/O1 Xplained Pro.
Todo:
Set sample rate to 100
kHz
Enable
Trigger on falling Edge
and set Mode to Normal
Push
Start in the DGI Control
Panel
Push the
Run-Stop button in the
Oscilloscope module
After some adjustments of the trigger level by dragging it with the mouse in the
oscilloscope plot area, and zooming in on the plot by adjusting the
Horizontal and Vertical range, a lamp
switch on event could look something like the picture below.By turning on the Cursors it is possible to measure the
time it takes for the lamp to settle in the ON state. In this case, it took about 300 ms
(ΔX in the plot area). Zooming further in on the plot makes
it possible to use the cursors to measure the frequency of the light flickering. The
1/ΔX field in the plot area shows that the frequency is about
100 Hz, which matches well with the 50 Hz AC power of the lamp (the power switches
polarity 100 times per second).