5.2.1.3 Run Example
To run the ADP example follow the steps below.
Todo:
- Open Atmel Studio
- Select File → New → Example Project
- Browse to, or search for the ADP example application - SAM D21 Xplained Pro and select it
- Choose the preferred folder and give the project a name, then click OK to create the project
The project will be generated, then it is just a matter of compiling it and programming it into the target board.
Todo:
- Open the project properties (right click the project in the Solution Explorer and select Properties)
- On the Tool tab, select the appropriate tool and interface
Todo:
- Click Start Without Debugging (Debug → Start Without Debugging)
Todo: Open
the Data Visualizer as an extension inside Atmel Studio by selecting it in the
Tools menu.
Todo:
- In the DGI Control Panel, select SAM D21 Xplained Pro
- Select the Autodetect protocols box
- Click Connect
You should see something like the screenshot below in the Data Visualizer.