3.4.3.1 Command Format (Host to BM70/71)
Note: The OPCODE field for the HCI Vendor
command is formatted as little endian. For the OPCODE (0x0406), byte[1] is 0x06, byte[2]
is 0x04.
|
Value of Parameter (4...5) |
Parameter Description |
Length – 2 Bytes |
|---|---|---|
0x0FFF | Connection handle | Format is little endian |
|
Value of Parameter (6) |
Parameter Description |
Length – 1 Byte |
|---|---|---|
0x00 | 0x00 – Programming complete 0x01 ... 0xFF – For more details on error codes, see Error Code Table Reference. With respect to programming, this value must always be zero from the host. | — |