13.1 Sleep Mode Operation
Sleep mode is entered by executing the SLEEP
         instruction.
Upon entering Sleep mode, the following conditions exist:
- Resets other than WDT are not affected by Sleep mode; WDT will be cleared but keeps running if enabled for operation during Sleep.
 - The PD bit is cleared.
 - The TO bit is set.
 - The CPU and the System clocks are disabled.
 - LFINTOSC and/or HFINTOSC will remain enabled if any peripheral has requested them as a clock source or if the HFOEN, MFOEN or LFOEN bits are set.
 - ADC is unaffected if the ADCRC oscillator is selected. When the
            ADC clock is something other than ADCRC, a 
SLEEPinstruction causes the present conversion to be aborted and the ADC module is turned off, although the ADON bit remains active. -  I/O ports maintain the status they had before
               
SLEEPwas executed (driving high, low, or high-impedance) only if no peripheral connected to the I/O port is active. 
Refer to individual sections for more details on peripheral operation during Sleep.
To minimize current consumption, the following conditions need to be considered:
- I/O pins will not be floating
 - External circuitry sinking current from I/O pins
 - Internal circuitry sourcing current from I/O pins
 - Current draw from pins with internal weak pull-ups
 - Modules using any oscillator
 
I/O pins that are high-impedance inputs need to be pulled to VDD or VSS externally to avoid switching currents caused by floating inputs.