5.1 TeraTerm Setup
(Ask a Question)The user application provides a user interface on the TeraTerm terminal through the UART interface.
To set up the TeraTerm program, perform the following steps:
- Ensure that the USB cable connects the host PC to the J5 (USB) port on the PolarFire Evaluation board.
- Start TeraTerm.
- Select Serial as the Connection type.
- Set the Serial
Port to the second highest COM port number from the drop-down
list, see the following figure. For example, COM9: FlashPro5 Port
[COM9] in this instance.
Figure 5-3. Select Serial as the Connection Type
Important: The COM port number is system specific. - In the TeraTerm
window, navigate to set;
- Baud rate: 115200
- Transmit delay: 5 msec/char and 5
msec/line
Rest of the serial port settings must be at default state, see the following figure, and click OK.
Figure 5-4. TeraTerm Configuration
This completes the TeraTerm program setup.