11 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

Table 11-1. Revision History
RevisionDateDescription
D03/2025Added Appendix 3: Programming the Device Using FlashPro Express section.
C02/2025The following is the list of changes in revision C of the document:
B04/2023In User Cryptoprocessor updated the text from "RSA, DSA, and modular exponentiation (Diffie-Hellman) with key sizes up to 4096-bits" to "RSA, DSA, and modular exponentiation (Diffie-Hellman) with key sizes up to 3072-bits".
A08/2022

The following is the list of changes in revision A of the document:

11.0—

The following is a summary of the changes made in this revision.

10.0—

Added Appendix 4: Running the TCL Script.

9.0—

In this revision, information about Prerequisites was updated.

8.0—

The following is a summary of the changes made in this revision.

  • Updated the document for Libero SoC v12.2.
  • Removed the references to Libero version numbers.
  • Added information about enabling protection for SPI Flash client. For more information, refer to LSRAM Initialization from SPI Flash.
7.0—

The following is a summary of the changes made in this revision.

6.0—

Updated the document for Libero SoC v12.0.

5.0—

The document was updated for Libero SoC PolarFire v2.3 release.

4.0—

The document was updated for Libero SoC PolarFire v2.2 release.

3.0—

The document was updated for Libero SoC PolarFire v2.1 release.

2.0—

The following is a summary of the changes made in this revision.

  • Information about initializing the SRAM component with the HEX file was added, see LSRAM Initialization from SPI Flash.
  • The document was updated to include features and enhancements introduced in the Libero SoC PolarFire v2.0 release.
1.0—

Initial release.