The RF trace from RFIOP (Pin #5) and
RFION (Pin #6) of the ATWILC3000A to the balun must be 50Ω differential controlled
impedance. The route from the balun to the antenna connector must be a 50Ω
controlled impedance trace. This trace must be routed in reference to the ground
plane. This ground reference plane must extend entirely under the ATWILC3000A QFN
package and to the sides of the these routes.
Discuss with the PCB vendor to get
the available PCB stack-ups and determine the trace dimensions for achieving 50Ω
single-ended controlled impedance.
Do not have any signal traces below/adjacent to the RF trace in the PCB.
Be sure that the RF traces from ATWILC3000A to the antenna are as short as possible to reduce path
losses and to mitigate the trace from picking up noise.
Place guard ground vias on either
side of the RF trace, running from module to the antenna feed point, in the
PCB.
Do not use thermal relief pads for the ground pads of all components in the RF path.
These component pads must be completely filled with GND copper polygon. Place
individual vias to the GND pads of these components.
It is recommended to have a 3x3 grid of ground vias solidly connecting the exposed
ground paddle of the ATWILC3000A to the ground plane on the inner/other layers of the
PCB. This will act as a good ground and thermal conduction path for the
ATWILC3000A.
Make sure that all digital signals
that may be toggling while the ATWILC3000A is active are placed as
far away from the antenna as possible.
Be sure to place the matching
components and balun as close to the RFIOP and RFION pins as possible (these are
C33, C23, C25, C17, C32, L8 and L9 in the reference schematic). The following figure
shows the placement and routing of these components.
Figure 11-1. Placement and Routing of Balun and Matching Components
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.