8 Testing of CoaXPress FMC Host with Basler Camera
(Ask a Question)To do CoaXPress FMC host testing with Basler camera, perform the following steps:
- Connect Basler camera to CoaXPress FMC host through Coax cable.
- Basler camera starts continuously blinking a green light. By default, the Basler camera streams Stream1.
- To see the video display on monitor, in the
CoaXPress - GenICam GUI Video Settings, set
Alpha to 255, as shown in the
following figure.
Figure 8-1. Using Basler Camera - To read XML, click Read XML.